AXIS#.SAFEPARAM.SDI.VELZEROWINDOW

Description

Indicates the velocity window of the safe direction (SDI) safety functions. This applies to both SDIp (positive) and SDIn (negative) functions.

Parameters Editor with the Velocity Zero Window row circled

 

This value is n_Zero_SDI in the following diagram:

Context

For complete SDI information refer to SDI (Safe Direction)

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDI.VELZEROWINDOW

3164h

09h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDI.VELZEROWINDOW

3264h

09h

Unsigned32

-

-

Read/Write

No